KEMET Announces New Automotive Grade Film Capacitors for Use in the Most Challenging Environments

F863 metallized polypropylene film capacitors provide robust, across-the-line filtering in automotive, industrial and mains-connected applications

GREENVILLE, S.C., Feb. 06, 2018 (GLOBE NEWSWIRE) -- KEMET Corporation (NYSE:KEM), a leading global supplier of electronic components, today announced a new family of automotive grade metallized polypropylene film capacitors. F863 class X2 miniature capacitors are specifically designed to provide robust performance in safety applications in harsh environments and severe ambient conditions.

KEMET F863 metallized polypropylene film capacitor
  F863 metallized polypropylene film capacitors provide robust, across-the-line filtering in automotive, industrial and mains-connected applications.


A photo accompanying this announcement is available at

These new devices address applications in both the automotive and industrial segments. They provide across-the-line EMI and RFI filtering for the growing number of vehicle electronics applications, as well as in mains-connected indoor applications such as capacitive power supplies.

The F863 series meets AEC-Q200 qualification requirements and is available in capacitance values ranging from 0.1 microfarads to 10 microfarads with rated voltages up to 310 VAC. The new, fully approved RFI X2 capacitors have an operating temperature range of -40 to +110 degrees Celsius.

The metallized polypropylene film dielectric exhibits excellent self-healing characteristics. Additionally, KEMET’s designers have enhanced the major components of this capacitor series to help resist traditional capacitance-loss mechanisms. With these improvements, the F863 series offers very high capacitance stability while meeting ENEC, CUL and CQC international safety requirements.

“The number and severity of challenging electrical and environmental applications is rising,” said Fabio Scagliarini, KEMET Vice President of Film Development. “The demand for complex vehicle electronics is increasing, and customers expect sensitive electronics products to work safely and reliably in high temperature, high humidity situations. Devices from KEMET’s F863 series can provide our customers a robust, dependable solution in these scenarios and comply with the prevailing industry standards.”

For more information, please visit


KEMET Corporation is a leading global manufacturer of electronic components that meet the highest standards for quality, delivery and service. The company offers its customers the broadest selection of capacitor technologies in the industry across all dielectrics, along with an expanding range of electromechanical devices, electromagnetic compatibility solutions and supercapacitors. KEMET’s corporate headquarters are in South Carolina; the company also operates manufacturing facilities, sales and distribution centers around the world. KEMET’s common stock is listed on the NYSE under the symbol “KEM.” Additional information about KEMET can be found at

Cautionary Statement on Forward-Looking Statements

Certain statements included herein contain forward-looking statements within the meaning of federal securities laws about KEMET Corporation's (the "Company") financial condition and results of operations that are based on management's current expectations, estimates and projections about the markets in which the Company operates, as well as management's beliefs and assumptions. Words such as "expects," "anticipates," "believes," "estimates," variations of such words and other similar expressions are intended to identify such forward-looking statements. These statements are not guarantees of future performance and involve certain risks, uncertainties and assumptions, which are difficult to predict. Therefore, actual outcomes and results may differ materially from what is expressed or forecasted in, or implied by, such forward-looking statements. Readers are cautioned not to place undue reliance on these forward-looking statements, which reflect management's judgment only as of the date hereof. The Company undertakes no obligation to update publicly any of these forward-looking statements to reflect new information, future events or otherwise.

Certain risks and uncertainties that could cause actual outcome and results to differ materially from those expressed in, or implied by, these forward-looking statements are described in the Company's reports and filings with the Securities and Exchange Commission.

Media Contact 

Dr. John C. Boan
Vice President, Marketing


Primary Logo


Source: KEMET Corporation