KEMET Enhances its Hi-Rel COTS KO-CAP® Polymer Electrolytic Device Offering with Extended Life Test Option

 

GREENVILLE, S.C., June 14, 2017 (GLOBE NEWSWIRE) -- KEMET Corporation (NYSE:KEM), a leading supplier of electronic components, has introduced the industry’s first COTS grade polymer electrolytic capacitor with a 1,000-hour life test option. The new option, also known as the “Biased Humidity Test,” provides capacitors qualified at 85 degrees Celsius with 85% relative humidity at rated voltage applied for 1,000 hours. The test type provides capacitors qualified to the rigors of MIL-STD-202 Method 103.

KEMET Enhances its Hi-Rel COTS KO-CAP® Polymer Electrolytic Device Offering with Extended Life Test Option
  KEMET has introduced the industry’s first COTS grade polymer electrolytic capacitor with a 1,000-hour life test option. The new option, also known as the “Biased Humidity Test,” provides capacitors qualified at 85 degrees Celsius with 85% relative humidity at rated voltage applied for 1,000 hours.

 

KEMET’s T540 COTS polymer electrolytic capacitors are typically used for decoupling in DC-DC converters or as hold-up capacitors in energy storage applications. Capacitance values up to 680 microfarads are available with the new extended life test option. Voltage ratings span 2.5 to 63 VDC and ESR specifications as low as twenty-five milliohms are available. The small surface mount form factor of the Hi-Rel COTS grade KO-CAP devices reduce board space requirements.

“Exposing polymer electrolytic capacitors to humidity had been a challenge. We first introduced the T598 automotive grade KO-CAP in 2015; now we are excited to offer a COTS grade KO-CAP that passes the same extended life test,” said Dr. Philip Lessner, Senior Vice President and Chief Technology Officer, KEMET. “This announcement is important because designers can take advantage of the polymer electrolytic technology in their high reliability and mission critical applications.”

For more information, please visit go.kemet.com/t540-85.

About KEMET

KEMET Corporation is a leading global supplier of electronic components. We offer our customers the broadest selection of capacitor technologies in the industry along with an expanding range of electromechanical devices, electromagnetic compatibility solutions and supercapacitors. Our vision is to be the preferred supplier of electronic component solutions demanding the highest standards of quality, delivery and service. KEMET’s common stock is listed on the NYSE under the symbol “KEM.” Additional information about KEMET can be found at http://www.kemet.com.

Cautionary Statement on Forward-Looking Statements

Certain statements included herein contain forward-looking statements within the meaning of federal securities laws about KEMET Corporation’s (the "Company") financial condition and results of operations that are based on management's current expectations, estimates and projections about the markets in which the Company operates, as well as management's beliefs and assumptions. Words such as "expects," "anticipates," "believes," "estimates," variations of such words and other similar expressions are intended to identify such forward-looking statements. These statements are not guarantees of future performance and involve certain risks, uncertainties and assumptions, which are difficult to predict. Therefore, actual outcomes and results may differ materially from what is expressed or forecasted in, or implied by, such forward-looking statements. Readers are cautioned not to place undue reliance on these forward-looking statements, which reflect management's judgment only as of the date hereof. The Company undertakes no obligation to update publicly any of these forward-looking statements to reflect new information, future events or otherwise.

Certain risks and uncertainties that could cause actual outcome and results to differ materially from those expressed in, or implied by, these forward-looking statements are described in the Company’s reports and filings with the Securities and Exchange Commission.

Contact:      
Dr. John C. Boan
Vice President, Marketing
johnnyboan@kemet.com
954.766.2813    

Contact for editors:
Simon Krelle, Publitek
Tel: +44 (0) 208 429 6553
E-mail: simon.krelle@publitek.com

Primary Logo

 

KEMET Corporation