KEMET is First Supplier to Offer Both Class-I and Class-II MLCCs Qualified to MIL-PRF-32535

 
Industry-Leading Base Metal Technology Enhances Ceramic Defense and Aerospace Portfolio  

FORT LAUDERDALE, Fla., June 18, 2018 (GLOBE NEWSWIRE) -- KEMET Corporation (NYSE:KEM), a leading global supplier of electronic components, today announced that it is the first and only supplier to offer both Class-I and Class-II base metal electrode (BME) multilayer ceramic capacitors (MLCCs) qualified for defense and aerospace applications by the Defense Logistics Agency (DLA). The DLA recently accepted KEMET's X7R dielectric MIL-PRF-32535 for "M" and "T" reliability levels.

KEMET MIL-PRF-32535 X7R Ceramic Capacitor
KEMET is the first and only supplier to offer both Class-I and Class-II base metal electrode (BME) multilayer ceramic capacitors (MLCCs) qualified for defense and aerospace applications by the Defense Logistics Agency (DLA). The DLA recently accepted KEMET's X7R dielectric MIL-PRF-32535 for "M" and "T" reliability levels.


MIL-PRF-32535 is the first DLA capacitor specification for defense and aerospace that capitalizes on industry-leading base metal electrode (BME) technology. In December 2017, KEMET announced DLA approval for C0G and BP Class-I dielectrics which are ideal for critical timing, tuning, pulse, AC, and transient voltage suppression applications where capacitance stability may be a concern. With the recent DLA approval of KEMET’s X7R Class-II dielectric, design engineers will now have access to ceramic capacitors that offer up to a 55-fold increase in capacitance values as compared to the offerings under traditional specifications using precious metal electrodes (PME). These capacitors are ideal for decoupling, bypass, filtering, and bulk storage for military, avionics and space applications.

MIL-PRF-32535 is also the first DLA specification to recognize a flexible termination option. KEMET's flexible termination utilizes a pliable conductive silver epoxy in the termination system. The addition of this epoxy layer inhibits the transfer of board stress to the rigid ceramic body, therefore mitigating flex cracks that can result in low insulation resistance or short circuit failures.

“KEMET has been a leader in BME ceramic capacitor development for over 20 years,” said Dr. Abhijit Gurav, KEMET Vice President of Ceramic Technology. “These new Class-I and Class-II capacitor ranges were qualified through the extremely stringent requirements of the MIL-PRF-32535 specification, and still offer significantly higher capacitance values than the MIL-PRF-123 and 55681 specifications. This enables more circuit functionality in defense and space applications while allowing significant component miniaturization and payload weight reduction.”

About KEMET

KEMET Corporation is a leading global manufacturer of electronic components that meet the highest standards for quality, delivery and service. The company offers its customers the broadest selection of capacitor technologies in the industry across all dielectrics, along with an expanding range of electromechanical devices, electromagnetic compatibility solutions and supercapacitors. KEMET’s corporate headquarters are in Florida; the company also operates manufacturing facilities, sales and distribution centers around the world. KEMET’s common stock is listed on the NYSE under the symbol “KEM.” Additional information about KEMET can be found at www.kemet.com.

Cautionary Statement on Forward-Looking Statements

Certain statements included herein contain forward-looking statements within the meaning of federal securities laws about KEMET Corporation’s (the "Company") financial condition and results of operations that are based on management's current expectations, estimates and projections about the markets in which the Company operates, as well as management's beliefs and assumptions. Words such as "expects," "anticipates," "believes," "estimates," variations of such words and other similar expressions are intended to identify such forward-looking statements. These statements are not guarantees of future performance and involve certain risks, uncertainties and assumptions, which are difficult to predict. Therefore, actual outcomes and results may differ materially from what is expressed or forecasted in, or implied by, such forward-looking statements. Readers are cautioned not to place undue reliance on these forward-looking statements, which reflect management's judgment only as of the date hereof. The Company undertakes no obligation to update publicly any of these forward-looking statements to reflect new information, future events or otherwise.

Certain risks and uncertainties that could cause actual outcome and results to differ materially from those expressed in, or implied by, these forward-looking statements are described in the Company’s reports and filings with the Securities and Exchange Commission.

Contact:      
Fernando Spada
Vice President, Marketing & Digital Engagement
fernandospada@kemet.com
954.766.2815                

A photo accompanying this announcement is available at http://www.globenewswire.com/NewsRoom/AttachmentNg/4c810765-4fa6-462a-bdd9-7f0009a4095e

Primary Logo

Source: KEMET Corporation