KEMET Introduces KC-LINK Capacitors for Fast-Switching Wide Bandgap Semiconductor Applications

 

SAN ANTONIO, March 05, 2018 (GLOBE NEWSWIRE) -- KEMET Corporation (NYSE:KEM), a leading global supplier of electronic components, today launched KC-LINK surface mount capacitors at APEC 2018 in San Antonio. KC-LINK is designed to meet the growing demand for fast-switching wide bandgap (WBG) semiconductors. Wide bandgap semiconductors have enabled power converters to operate at higher voltages, temperatures, and frequencies, allowing for much higher efficiencies and power densities.

KC-LINK Capacitors for Fast-Switching Wide Bandgap Semiconductor Applications
  KEMET KC-LINK capacitors are designed to meet the growing demand for fast-switching wide bandgap (WBG) semiconductors

 

KC-LINK capacitors can operate at very high ripple currents due to superior capacitance stability over temperature and voltage, rendering them ideal for DC link, snubber and resonator applications. This is due to KEMET’s robust and proprietary C0G/NPO base metal electrode (BME) dielectric system, which operates with very low effective series resistance (ESR) and thermal resistance. With an operating temperature of 150°C, these capacitors can be mounted close to fast-switching semiconductors in high power density applications which require minimal cooling. 

“The low ESR of KC-LINK capacitors results in best-in-class ripple current capability,” said John Bultitude, KEMET Vice President and Technical Fellow. “Combined with their thermal stability and mechanical robustness, KC-LINK is excellent for assembly close to hot WBG semiconductors where it is difficult to actively cool parts.”

High mechanical robustness allows KC-LINK capacitors to be mounted without the use of lead frames. This provides extremely low effective series inductance (ESL), increasing the operating frequency range and allowing for further miniaturization. Available in both commercial and automotive grades with standard and flexible termination systems, this series is Pb-Free, RoHS and REACH compliant. For more information, please visit KEMET at APEC booth 309, or www.kemet.com/KC-LINK.

About KEMET
KEMET Corporation is a leading global manufacturer of electronic components that meet the highest standards for quality, delivery and service. The company offers its customers the broadest selection of capacitor technologies in the industry, along with an expanding range of sensors, actuators, and electromagnetic compatibility solutions. KEMET operates manufacturing facilities, sales and distribution centers around the world. The company’s common stock is listed on the NYSE under the symbol “KEM.” Additional information about KEMET can be found at www.kemet.com.

Cautionary Statement on Forward-Looking Statements

Certain statements included herein contain forward-looking statements within the meaning of federal securities laws about KEMET Corporation’s (the "Company") financial condition and results of operations that are based on management's current expectations, estimates and projections about the markets in which the Company operates, as well as management's beliefs and assumptions. Words such as "expects," "anticipates," "believes," "estimates," variations of such words and other similar expressions are intended to identify such forward-looking statements. These statements are not guarantees of future performance and involve certain risks, uncertainties and assumptions, which are difficult to predict. Therefore, actual outcomes and results may differ materially from what is expressed or forecasted in, or implied by, such forward-looking statements. Readers are cautioned not to place undue reliance on these forward-looking statements, which reflect management's judgment only as of the date hereof. The Company undertakes no obligation to update publicly any of these forward-looking statements to reflect new information, future events or otherwise.

Certain risks and uncertainties that could cause actual outcome and results to differ materially from those expressed in, or implied by, these forward-looking statements are described in the Company’s reports and filings with the Securities and Exchange Commission.

Contact:      
Dr. John C. Boan
Vice President, Marketing
johnnyboan@kemet.com 
954.766.2813                 

A photo accompanying this announcement is available at http://www.globenewswire.com/NewsRoom/AttachmentNg/1af7e0a6-1666-4cc1-9056-95582892dc51

 

Primary Logo

 

Source: KEMET Corporation