KEMET Introduces KPS-MCC C0G High Temperature 200 Degree Celsius Bulk Capacitance Solution for Harsh Environment Applications
GREENVILLE, S.C.,
|
A photo accompanying this announcement is available at http://www.globenewswire.com/NewsRoom/AttachmentNg/a1aeeacb-0843-40c0-95f4-a93a86e02a45
The KEMET C0G BME dielectric system is designed to provide high reliability at operating temperatures up to 200 degrees Celsius, while maintaining high insulation resistance, very low ESR and very high ripple current capability at high frequencies. In addition, this series provides superior stability with no capacitance change versus DC voltage and ±30 ppm/°C capacitance change over temperature. A high melting point (HMP) solder for lead attachment enables multiple chips to be stacked in parallel to provide bulk capacitance with excellent mechanical robustness. Superior electrical performance, high reliability, and mechanical robustness of KEMET’s BME C0G dielectric results in a preferred solution over Class II (X7R/X5R) capacitors above 175 degrees Celsius.
Available in three case sizes, the KPS-MCC series offers voltages up to 2,000 V and capacitance up to 2 microfarads in a footprint of less than 0.55 square inches. Each case size can be ordered in a straight pin, formed “L,” or formed “J” configuration and with a silver (Ag) or solder coated (SnPb) termination finish.
“This latest addition to KEMET’s world-class BME C0G offering extends KEMET’s portfolio up to 2 microfarads in a Class I solution,” said Dr. John Bultitude, KEMET Vice President and Technical Fellow. “With KEMET’s temperature-cycling resistant lead frame technology and high ripple current capability, these bulk capacitance solutions provide unparalleled performance for the harshest environments on, under and above the Earth.”
For more information, please visit http://www.kemet.com/Hi-Temp-Ceramic.
About KEMET
Cautionary Statement on Forward-Looking Statements
Certain statements included herein contain forward-looking statements within the meaning of federal securities laws about KEMET Corporation’s (the "Company") financial condition and results of operations that are based on management's current expectations, estimates and projections about the markets in which the Company operates, as well as management's beliefs and assumptions. Words such as "expects," "anticipates," "believes," "estimates," variations of such words and other similar expressions are intended to identify such forward-looking statements. These statements are not guarantees of future performance and involve certain risks, uncertainties and assumptions, which are difficult to predict. Therefore, actual outcomes and results may differ materially from what is expressed or forecasted in, or implied by, such forward-looking statements. Readers are cautioned not to place undue reliance on these forward-looking statements, which reflect management's judgment only as of the date hereof. The Company undertakes no obligation to update publicly any of these forward-looking statements to reflect new information, future events or otherwise.
Certain risks and uncertainties that could cause actual outcome and results to differ materially from those expressed in, or implied by, these forward-looking statements are described in the Company’s reports and filings with the
Contact:
Dr. John C. Boan
Vice President, Marketing
johnnyboan@kemet.com
954.766.2813
Source: KEMET Corporation