KEMET Introduces Two New Series of Power Film Capacitors for Increasingly Demanding High Power, High Frequency Applications

 

NUREMBERG, Germany, June 05, 2018 (GLOBE NEWSWIRE) -- KEMET Corporation (NYSE:KEM), a leading global supplier of electronic components, today announced two new series of power film capacitors that meet the requirements of AEC-Q200. The C4AQ series is suited for industrial, automotive and power supply designs for DC link, DC filtering and energy storage applications, while the C4AF series addresses similar applications, but is specifically designed for harsh environments.

KEMET's new series of power film capacitors meet the requirements of AEC-Q200.
  The C4AQ series is suited for industrial, automotive and power supply designs for DC link, DC filtering and energy storage applications, while the C4AF series addresses similar applications, but is specifically designed for harsh environments

 

The new RoHS compliant capacitors have a polypropylene metallized film construction and are available as two or four radial leaded board mount devices. Available values for the C4AQ series range from 1.0 µF to 130 µF, with additional sampling for 170 µF and 210 µF. Voltage values span from 500 VDC to 1500 VDC. Devices from the C4AF series are designed for use in more demanding and harsh applications and are offered in capacitance values up to 62 µF with voltage ratings up to 400 VAC.

AEC-Q200 qualified devices within the C4AQ and C4AF ranges address the requirements of the increasing amounts of electronic content in automotive applications, where operating environments can be particularly challenging from both an electrical and environmental standpoint.

KEMET’s new power film capacitors are well suited for increasingly common high frequency applications. The capacitors are housed in rectangular, resin filled enclosures and deliver an array of application benefits including self-healing characteristics and low losses. High ripple current values, high capacitance density and high contact reliability are additional features of the new devices. The operating temperature range of the power film capacitors is -55°C to +105°C.

“Our new power film capacitors have been developed to provide a robust and reliable solution in high power, high frequency applications for challenging end uses,” said Fabio Scagliarini, KEMET Vice President of Film and Filter Business Development. “We continue to leverage our extensive experience and technical expertise to design and introduce capacitive and other passive component solutions that address the evolving and increasingly stringent demands of the automotive and industrial sectors.”

Visitors to PCIM Europe (June 5 – 7, Nuremberg) can see the new capacitors, plus KEMET’s wide range of component solutions at Hall 9, Stand 403.

About KEMET
KEMET Corporation is a leading global manufacturer of electronic components that meet the highest standards for quality, delivery and service. The company offers its customers the broadest selection of capacitor technologies in the industry, along with an expanding range of sensors, actuators and electromagnetic compatibility solutions. KEMET operates manufacturing facilities, sales and distribution centers around the world. The company’s common stock is listed on the NYSE under the symbol “KEM.” Additional information about KEMET can be found at www.kemet.com.

Cautionary Statement on Forward-Looking Statements

Certain statements included herein contain forward-looking statements within the meaning of federal securities laws about KEMET Corporation’s (the "Company") financial condition and results of operations that are based on management's current expectations, estimates and projections about the markets in which the Company operates, as well as management's beliefs and assumptions. Words such as "expects," "anticipates," "believes," "estimates," variations of such words and other similar expressions are intended to identify such forward-looking statements. These statements are not guarantees of future performance and involve certain risks, uncertainties and assumptions, which are difficult to predict. Therefore, actual outcomes and results may differ materially from what is expressed or forecasted in, or implied by, such forward-looking statements. Readers are cautioned not to place undue reliance on these forward-looking statements, which reflect management's judgment only as of the date hereof. The Company undertakes no obligation to update publicly any of these forward-looking statements to reflect new information, future events or otherwise.

Certain risks and uncertainties that could cause actual outcome and results to differ materially from those expressed in, or implied by, these forward-looking statements are described in the Company’s reports and filings with the Securities and Exchange Commission.

Contact:      
Fernando Spada
Vice President, Marketing & Digital Engagement
fernandospada@kemet.com
954.766.2815   

A photo accompanying this announcement is available at http://www.globenewswire.com/NewsRoom/AttachmentNg/61c223ae-4528-4140-98ad-a529be3aa9e5

Primary Logo

 

Source: KEMET Corporation