KEMET Releases New Capacitor Families Built with Advanced Materials for Superior Reliability and Space Savings

 
KEMET's new surface mount conductive polymer aluminum solid electrolytic capacitors feature very low ESR resulting in low self-heating and high ripple current capability.
KEMET's new through-hole conductive polymer aluminum solid electrolytic capacitors leverage the latest high-conductivity polymer for superior reliability and space-savings.

MUNICH, GERMANY--(Marketwired - November 08, 2016) - KEMET Corporation (NYSE: KEM), a leading global supplier of electronic components, announced six new families of surface mount and through-hole conductive polymer aluminum solid electrolytic capacitors, with voltage ratings up to 250 VDC. Leveraging KEMET's latest high-conductivity polymer, the new devices have very low equivalent series resistance (ESR) resulting in low self-heating and high ripple-current capability.

The high ripple current capability allows these new devices to replace arrays of multiple conventional electrolytic capacitors connected in parallel, thereby enabling designers to save PCB real estate. In addition, the new families deliver enhanced reliability by giving ten-times longer life for every 20°C reduction in operating temperature. Conventional capacitors give only double the lifetime for every 10°C reduction, according to conventional guidelines.

The through-hole devices cover capacitance values from 2.2 to 1,500 microfarads, in four families that give designers a choice of properties including 2.5-250 VDC operating voltage range, extended lifetime of up to 5,000 hours, and -55°C to 125°C specified-temperature range.

The surface-mount families feature operating voltage up to 50 VDC, specified-temperature range of -55°C to 105°C, rated lifetime of 2,000 hours, and capacitance values between 10 and 2,700 microfarads.

For more information, please visit www.kemet.com/alpolymer, or the KEMET mobile apps for iPad®, iPhone®, Android™ and Windows®.

About KEMET

KEMET Corporation is a leading global manufacturer of electronic components that meet the highest standards for quality, delivery and service. The company offers its customers the broadest selection of capacitor technologies in the industry across all dielectrics, along with an expanding range of electromechanical devices, electromagnetic compatibility solutions and supercapacitors. KEMET's corporate headquarters are in South Carolina; the company also operates manufacturing facilities, sales and distribution centers around the world. KEMET's common stock is listed on the NYSE under the symbol "KEM." Additional information about KEMET can be found at www.kemet.com.

Cautionary Statement on Forward-Looking Statements

Certain statements included herein contain forward-looking statements within the meaning of federal securities laws about KEMET Corporation's (the "Company") financial condition and results of operations that are based on management's current expectations, estimates and projections about the markets in which the Company operates, as well as management's beliefs and assumptions. Words such as "expects," "anticipates," "believes," "estimates," variations of such words and other similar expressions are intended to identify such forward-looking statements. These statements are not guarantees of future performance and involve certain risks, uncertainties and assumptions, which are difficult to predict. Therefore, actual outcomes and results may differ materially from what is expressed or forecasted in, or implied by, such forward-looking statements. Readers are cautioned not to place undue reliance on these forward-looking statements, which reflect management's judgment only as of the date hereof. The Company undertakes no obligation to update publicly any of these forward-looking statements to reflect new information, future events or otherwise.

Certain risks and uncertainties that could cause actual outcome and results to differ materially from those expressed in, or implied by, these forward-looking statements are described in the Company's reports and filings with the Securities and Exchange Commission.

Image Available: http://www.marketwire.com/library/MwGo/2016/11/4/11G120858/Images/Aluminum_A765_Main-e08e762098239d5891a61a3107591333.JPG
Image Available: http://www.marketwire.com/library/MwGo/2016/11/4/11G120858/Images/Aluminum_A759_Main-d53976d28f42bd5c98b138c41c183c47.JPG

 

 

Contact:
Dr. John C. Boan
Vice President, Marketing
johnnyboan@kemet.com