KEMET Introduces KO-CAP® Reliability Assessment Method

 

GREENVILLE, S.C., Dec. 1, 2015 // -- KEMET Corporation (NYSE: KEM), a leading global supplier of electronic components, introduced its new KO-CAP® Reliability Assessment method, the first of its kind for polymer electrolytic capacitors.

The KEMET T540 and T541 Commercial-Off-the-Shelf (COTS) Series are the only polymer electrolytic capacitors available today with failure rate options defined by the new KO-CAP Reliability Assessment method.

The T540 and T541 Commercial-Off-the-Shelf (COTS) Series are the only polymer electrolytic capacitors available today with failure rate options defined by this innovative testing criteria. Developed as a result of over ten years of research, the Reliability Assessment method utilizes accelerated voltage and temperature conditions applied to board-mounted samples to assess long-term device reliability. The failure rates available are B (0.1% per 1,000 hours), C (0.01% per 1,000 hours) and D (0.001% per 1,000 hours).

This new Reliability Assessment method complements the successful T540 and T541 COTS Series KO-CAPs. These high performance capacitors are designed for decoupling and filtering applications that require very low equivalent series resistance (ESR). By utilizing an organic conductive polymer as the cathode plate of the capacitor, this technology results in low ESR, high ripple current capability and improved capacitance retention at high frequency. Such performance characteristics are ideal for various high reliability defense and aerospace applications such as radar, sonar, power supplies and guidance systems. KO-CAPs with the new Reliability Assessment method are available with rated voltages from 2.5 to 63 VDC, capacitances up to 1,500 µF, and ESR as low as 5 milliohms – all in surface mount packaging.

Design engineers can now match the reliability requirements of their project to the appropriate failure rate. Traditional Weibull methods of assessing reliability are not suitable for polymer electrolytic capacitors and fall short of properly assessing lot-to-lot reliability. Prior to this release, this capability was only available through source control drawings, but is now easy to design in by adding the desired failure rate to the 13th character of the part number.

For more information on KEMET's KO-CAP Reliability Assessment method, please visit www.kemet.com/KOCAP-ER

About KEMET
KEMET Corporation is a leading global supplier of electronic components. We offer our customers the broadest selection of capacitor technologies in the industry, along with an expanding range of electromechanical devices, electromagnetic compatibility solutions and supercapacitors. Our vision is to be the preferred supplier of electronic component solutions demanding the highest standards of quality, delivery and service. KEMET's common stock is listed on the NYSE under the symbol "KEM." Additional information about KEMET can be found at http://www.kemet.com.

Cautionary Statement on Forward-Looking Statements

Certain statements included herein contain forward-looking statements within the meaning of federal securities laws about KEMET Corporation's (the "Company") financial condition and results of operations that are based on management's current expectations, estimates and projections about the markets in which the Company operates, as well as management's beliefs and assumptions. Words such as "expects," "anticipates," "believes," "estimates," variations of such words and other similar expressions are intended to identify such forward-looking statements. These statements are not guarantees of future performance and involve certain risks, uncertainties and assumptions, which are difficult to predict. Therefore, actual outcomes and results may differ materially from what is expressed or forecasted in, or implied by, such forward-looking statements. Readers are cautioned not to place undue reliance on these forward-looking statements, which reflect management's judgment only as of the date hereof. The Company undertakes no obligation to update publicly any of these forward-looking statements to reflect new information, future events or otherwise.

Certain risks and uncertainties that could cause actual outcome and results to differ materially from those expressed in, or implied by, these forward-looking statements are described in the Company's reports and filings with the Securities and Exchange Commission.

Contact:

Dr. John C. Boan

 

Vice President, Marketing

johnnyboan@kemet.com

954.766.2813           

Photo - http://photos.prnewswire.com/prnh/20151201/292219

SOURCE KEMET Corporation